Latest news
New S8NR IP67 power supply with built-in diagnostics for machine-mounted power circuits
20 July, 2026 The S8NR IP67-rated power supply series from OMRON is designed to be mounted directly on machinery, outside the control panel. It spans 90 W to 600 W (24 V DC), and the 360 W and 600 W models pack up to six individually protected outputs into a single unit. This reduces the number of separate parts an engineer needs to select and wire. Alongside the S8NR, OMRON has also introduced the IP67-rated S8R-BB DC Blocking Box, which lets control circuits be wired outside the panel too.
From shop floor to smart factory: OMRON i-BELT service delivers end-to-end manufacturing transformation with measurable results
29 June, 2026 Purpose-built to end the cycle of failed pilots, the service combines lean manufacturing expertise, IT-OT integration and full project ownership, to achieve even more than 30% OEE improvement.
-
OMRON at interpack
Booth impressions from interpack 2026, world's leading trade fair for the packaging industry
00:25
Integrated automation innovation at interpack 2026
03 June, 2026 OMRON presents integrated automation innovation at interpack 2026
Comau and OMRON Robotics collaborate to accelerate advanced industrial automation across high-growth manufacturing sectors
11 May, 2026 Combining complementary robotics, control, and software capabilities to deliver flexible, scalable automation solutions for global customers.
-
OMRON OL-450S autonomous mobile robot with new mast configuration options
OMRON has expanded the OL-450S line-up with new mast configurations, giving operators and integrators greater control over how the robot navigates and localizes in their specific environments. The OL-450S is available with no mast, short mast, or tall mast configurations. For highly dynamic areas, OMRON also offers a tower mast accessory that positions the localization laser above floor-level clutter, improving robustness where obstacles, staging areas, or layouts change frequently.
02:49
OMRON introduces new mast configuration options for OL-450S AMR
07 May, 2026 OMRON has announced expanded configuration options for its OL-450S Autonomous Mobile Robot (AMR), adding new mast options for cart and load carrier transport across production and intralogistics operations. At interpack 2026, OMRON gives visitors a first-hand look at one of the new options in action, with a live demonstration at the Packaging Valley booth in Hall 16, Stand D72-11. The demonstration also features the OL-450S with an integrated VHV5 QR code reader, showing how mobile robotics can be combined with sensing and identification technologies to support enhanced tracking in workflows.
OMRON and Dassault Systèmes Partner to Bridge the Virtual and the Real Worlds for Flexible, High-Performance Manufacturing
21 April, 2026 OMRON and Dassault Systèmes combine their respective expertise in virtual twins and industrial automation technologies to transform industrial production.
OMRON Appoints Virendra Shelar as President and CEO of its Industrial Automation Business in EMEA
01 April, 2026 OMRON has appointed Virendra Shelar as Executive Officer, President and CEO of OMRON EUROPE B.V., effective 1 April 2026. He will be based at OMRON's European headquarters in Hoofddorp, the Netherlands.
OMRON earns top 5% ranking in EcoVadis sustainability assessment
30 March, 2026 OMRON Corporation has earned a Gold rating from EcoVadis, placing it in the top 5% for sustainability performance.
New VHV5 inline verifier from OMRON for real-time, ISO-compliant barcode quality control
10 March, 2026 OMRON has introduced the VHV5 inline verifier, a high-speed barcode verification system designed to verify 1D, 2D, and Direct Part Mark (DPM) codes directly on the production line. The VHV5 performs real-time verification of Code 128, Data Matrix, QR Codes, and DPM marks at speeds of up to 1,000 codes per minute, ensuring that every code applied during marking or printing is readable, compliant, and traceable.
OMRON’s S8AS2 smart power supply integrates power, protection, and diagnostics in one unit
10 February, 2026 OMRON has announced the launch of the S8AS2 smart power supply, an innovative and compact solution that combines DC power supply, electronic circuit protection, and real-time monitoring in a single, panel-mountable unit. The S8AS2 is designed for factory automation and industrial control panels, helping reduce panel space requirements, wiring complexity, and downtime.
OMRON introduces new high-payload collaborative robots and TMflow software upgrade
12 January, 2026 OMRON Robotics and Safety Technologies has expanded its TM S Series collaborative robot portfolio with three new models and a major software update, supporting manufacturers facing labour shortages and increasing requirements for flexible, high-mix production. The TM30S, TM20S and TM6S extend the series’ payload and reach capabilities for applications such as palletising, machine tending and precision handling.
New S8NR IP67 power supply with built-in diagnostics for machine-mounted power circuits
20 July, 2026 The S8NR IP67-rated power supply series from OMRON is designed to be mounted directly on machinery, outside the control panel. It spans 90 W to 600 W (24 V DC), and the 360 W and 600 W models pack up to six individually protected outputs into a single unit. This reduces the number of separate parts an engineer needs to select and wire. Alongside the S8NR, OMRON has also introduced the IP67-rated S8R-BB DC Blocking Box, which lets control circuits be wired outside the panel too.
-
OMRON OL-450S autonomous mobile robot with new mast configuration options
OMRON has expanded the OL-450S line-up with new mast configurations, giving operators and integrators greater control over how the robot navigates and localizes in their specific environments. The OL-450S is available with no mast, short mast, or tall mast configurations. For highly dynamic areas, OMRON also offers a tower mast accessory that positions the localization laser above floor-level clutter, improving robustness where obstacles, staging areas, or layouts change frequently.
02:49
OMRON introduces new mast configuration options for OL-450S AMR
07 May, 2026 OMRON has announced expanded configuration options for its OL-450S Autonomous Mobile Robot (AMR), adding new mast options for cart and load carrier transport across production and intralogistics operations. At interpack 2026, OMRON gives visitors a first-hand look at one of the new options in action, with a live demonstration at the Packaging Valley booth in Hall 16, Stand D72-11. The demonstration also features the OL-450S with an integrated VHV5 QR code reader, showing how mobile robotics can be combined with sensing and identification technologies to support enhanced tracking in workflows.
New VHV5 inline verifier from OMRON for real-time, ISO-compliant barcode quality control
10 March, 2026 OMRON has introduced the VHV5 inline verifier, a high-speed barcode verification system designed to verify 1D, 2D, and Direct Part Mark (DPM) codes directly on the production line. The VHV5 performs real-time verification of Code 128, Data Matrix, QR Codes, and DPM marks at speeds of up to 1,000 codes per minute, ensuring that every code applied during marking or printing is readable, compliant, and traceable.
OMRON’s S8AS2 smart power supply integrates power, protection, and diagnostics in one unit
10 February, 2026 OMRON has announced the launch of the S8AS2 smart power supply, an innovative and compact solution that combines DC power supply, electronic circuit protection, and real-time monitoring in a single, panel-mountable unit. The S8AS2 is designed for factory automation and industrial control panels, helping reduce panel space requirements, wiring complexity, and downtime.
OMRON introduces new high-payload collaborative robots and TMflow software upgrade
12 January, 2026 OMRON Robotics and Safety Technologies has expanded its TM S Series collaborative robot portfolio with three new models and a major software update, supporting manufacturers facing labour shortages and increasing requirements for flexible, high-mix production. The TM30S, TM20S and TM6S extend the series’ payload and reach capabilities for applications such as palletising, machine tending and precision handling.
OMRON introduces FHV7-AI Detection Camera to simplify AI-based quality control
03 November, 2025 The FHV7-AI Detection Camera is the latest addition to OMRON’s proven family of industrial vision systems. The new model combines advanced AI-driven inspection capabilities with a simplified, step-by-step user interface and a compact, all-in-one design – reducing engineering time and overall cost of ownership. This allows manufacturers and machine builders to implement high-accuracy inspection without complex setup or specialized expertise, or inflated product budgets
OMRON launches M1-EMP AC Drive with multiprotocol Ethernet support
27 October, 2025 OMRON has expanded its M1 Compact AC Drives family with the new M1-EMP (Ethernet Multi Protocol) model. AC drives, often referred to as inverters, are a core component of industrial automation, controlling the speed, torque, and position of electric motors in machines and production systems. They help manufacturers improve energy efficiency, achieve precise motion control, and adapt equipment to changing process demands.
OMRON Introduces DX1 Data Flow Controller
17 October, 2025 Easy-to-use industrial edge controller for fast and reliable on-site data utilization and visualization
OMRON enhances FH Vision System with improved AI features
01 October, 2025 OMRON has announced an important new update to its FH Vision System that eliminates over-detection, and delivers fast, reproducible results, even on textured, reflective, or variable surfaces. This makes it easier than ever for manufacturers to achieve reliable, high-precision defect detection in challenging environments, whilst benefiting from a perpetual license for long-term use.
-
Meet the OL-450S Autonomous Mobile Robot
Discover the latest addition to the OMRON AMR Family: OL-450S, a versatile and efficient autonomous mobile robot designed to maximize efficiency of cart transport operations, perfect for lineside replenishment operations with advanced safety technology. The OL-450S is built to streamline material transport with a 450 kg payload capacity, adjustable lift height, advanced navigation, and wireless charging. Capable of handling roll cages, pick carts, pallets, and trolleys, the OL-450S integrates seamlessly with OMRON’s FLOW Core software ecosystem for efficient fleet management and reliable performance in high-traffic environments. With 360° safety coverage and a fully integrated, ready-to-deploy design, the OL-450S eliminates the need for customizations. Discover more: #MakeitOMRON #mobilerobots #autonomousmobilerobots
03:25
OMRON introduces the OL-450S – A complete autonomous mobile robot solution for material handling
01 May, 2025 OMRON has released the OL-450S, a low-profile, omni-directional autonomous mobile robot (AMR) designed to optimize workflows, maximize efficiency, and improve safety in material handling.
OMRON expands inverter portfolio with the launch of the new J1 inverter
14 April, 2025 OMRON has launched the new J1 inverter, a compact and cost-effective solution designed for low-end applications where space, reliability and price are decisive factors.
From shop floor to smart factory: OMRON i-BELT service delivers end-to-end manufacturing transformation with measurable results
29 June, 2026 Purpose-built to end the cycle of failed pilots, the service combines lean manufacturing expertise, IT-OT integration and full project ownership, to achieve even more than 30% OEE improvement.
-
OMRON at interpack
Booth impressions from interpack 2026, world's leading trade fair for the packaging industry
00:25
Integrated automation innovation at interpack 2026
03 June, 2026 OMRON presents integrated automation innovation at interpack 2026
Comau and OMRON Robotics collaborate to accelerate advanced industrial automation across high-growth manufacturing sectors
11 May, 2026 Combining complementary robotics, control, and software capabilities to deliver flexible, scalable automation solutions for global customers.
OMRON and Dassault Systèmes Partner to Bridge the Virtual and the Real Worlds for Flexible, High-Performance Manufacturing
21 April, 2026 OMRON and Dassault Systèmes combine their respective expertise in virtual twins and industrial automation technologies to transform industrial production.
OMRON Appoints Virendra Shelar as President and CEO of its Industrial Automation Business in EMEA
01 April, 2026 OMRON has appointed Virendra Shelar as Executive Officer, President and CEO of OMRON EUROPE B.V., effective 1 April 2026. He will be based at OMRON's European headquarters in Hoofddorp, the Netherlands.
OMRON earns top 5% ranking in EcoVadis sustainability assessment
30 March, 2026 OMRON Corporation has earned a Gold rating from EcoVadis, placing it in the top 5% for sustainability performance.
OMRON Awarded Newsweek's World's Greenest Companies 2025
24 November, 2025 OMRON secures 5-star rating for sustainability targets and on-going decarbonization initiatives around the world
Automation in motion: OMRON’s European tour returns this autumn
11 September, 2025 OMRON Industrial Automation is pleased to announce the continuation of its exclusive European tour on Automation Excellence. Following a successful start earlier this year, the tour will resume in Italy in October and then travel to Iberia, the Nordics, the UK, and Eastern Europe.
OMRON's Automation Center in Stuttgart receives iF Design Award 2025
02 June, 2025 OMRON has been recognised with a 2025 iF Design Award for its new Automation Center in Stuttgart, Germany. The award, presented by the iF International Forum Design GmbH, highlights the Automation Center's thoughtful design and its contribution to collaborative industrial innovation.
OMRON selected as one of the Top 100 Global Innovators 2025
06 May, 2025 OMRON Corporation has been recognized as one of the Top 100 Global Innovators 2025 by Clarivate. This marks OMRON’s tenth overall selection and the ninth consecutive year the company has received this recognition.