Latest news | OMRON, Europe

Login

We are experiencing technical difficulties. Your form submission has not been successful. Please accept our apologies and try again later. Details: [details]

Download

Register

We are experiencing technical difficulties. Your form submission has not been successful. Please accept our apologies and try again later. Details: [details]
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
We are experiencing technical difficulties. Your form submission has not been successful. Please accept our apologies and try again later. Details: [details]

Download

Thank you for your interest

You now have access to Latest news

A confirmation email has been sent to

Continue to page

Please or get direct access to download this document

Latest news

product
Introducing OMRON HD-1500 Mobile Robot
  • Introducing OMRON HD-1500 Mobile Robot

    Introducing OMRON HD-1500 Mobile Robot

    Introducing OMRON’s strongest mobile robot: the HD-1500. The HD-1500 is an advanced autonomous mobile robot specifically designed to transport heavy payloads up to 1500 kilograms. The HD-1500 also represents innovations in mobile robotics. Its new architecture features lasers that provide 360-degree safety coverage, as well as an onboard programmable logic controller, or PLC, to easily interface with custom attachments. Heavier payloads, built-in controller, improved sensors, route planning and object avoidance, the OMRON HD-1500 autonomous mobile robot offers the most advanced performance and safety. Learn more:

    03:00

New HD-1500 mobile robot with 1500kg payload capacity

July 22, 2020 Industry-leading HD-1500 expands the possibilities for autonomous material transport
READ MORE
corporate
business technology concept iot information communication network fcard peop

Delivery information

May 01, 2020 We are committed to maintaining business continuity towards our customers, suppliers and partners to manage these challenging times and get through this global crisis.
READ MORE
product
Bigger, stronger, better: new LD-250 mobile robot from Omron moves payloads up to 250kg
  • Bigger, stronger, better: new LD-250 mobile robot from Omron moves payloads up to 250kg

    Bigger, stronger, better: new LD-250 mobile robot from Omron moves payloads up to 250kg

    The new LD-250 mobile robot from Omron can handle a payload of 250kg and is the strongest and newest addition to our LD series of mobile robots. Together with the Fleet Manager, which for the first time in the industry enables the control of multiple mobile robots with different payloads through one system, it will help realize a more flexible and optimized autonomous material transport system.

    02:37

New LD-250 mobile robot to move payloads up to 250kg

November 15, 2019 Industry first to control different types of mobile robots via one system.
READ MORE
product
Component Focus: Omron Wireless Buttons
  • Component Focus: Omron Wireless Buttons

    Component Focus: Omron Wireless Buttons

    I'm Josh Bishop for cooling. It takes a wide voltage input from 100 to 240 volts AC and accepts either 50 or 60 Hertz. You can connect the incoming power here at the bottom with line, neutral and ground inputs. This particular power supply outputs the 24 volt DC power at the top with these terminal blocks and can provide up to 15 watts which is ample power for this wireless receiver or many other devices. There are other S8V caged power supplies that can output more power, but this works great in this case. The S8VK is providing power to this wireless receiver the A2W-RPC- WC1. This receiver is very straightforward to use with clearly marked ports and switches and common sense usage. This has eight outputs and accordingly can be synced with eight wireless buttons. You can see the power input up at the top and the outputs here at the bottom. There are lights for power, any potential errors and receipt of signals right here. There's also a slide switch for usage testing and setup. You'll note that this is 922.5 megahertz which gives it a greater range and better signal propagation than higher frequency signals. We end up with the communication assistance of about 100 meters without any obstructions. Finally we have the two push-button switches. They're obviously both wireless and they generate their own power so no battery is required. This also eliminates the need for maintenance. A light comes on when you click the button showing that it has been actuated and is working. They come with the space to allow you to easily mount them and swap them around as you need. The buttons are functionally the same, but you have the option of different types of plungers depending on what works best in your situation. They're both ULl certified, rated up to 1 million operations and are IP65 sealed. They're also shock and vibration resistant making them ideal for tough industrial application. All of this is connected and powered up. It is not set up and I'll walk you through the process just to show you how easy it is for you. You'll need to connect the S8VK to power. Again it can use power from practically anywhere in the world. Then hook the output of the power supply to the input of the wireless receiver and now everything will turn on and you'll be up to the point where I am currently. Programming the buttons and the receiver doesn't require anything external like a computer, you simply set the rotary switch to the channel you want to use, move the slide switch to ID and then click the button you want to use, 3 times relatively quickly. You'll see the receive light come on indicating that the receiver got the message and it has been paired. Switch to another channel do the same thing with the other button. That's it! It's recommended to make certain other systems in the area are not in use during this procedure, however, as it may cause problems. Let's move the slider switch to run and start clicking these buttons and watch those different indicators light up. Now deleting the buttons and reassigning them is just as easy; put the rotary switched to delete and click the button three times until the light comes on. The button is now unassigned and can be programmed to another output slot. With just a few components in a couple minutes of setup you can easily integrate Omron's wireless buttons into your systems. if you want to learn more or purchase these Omron components go to Features: - 8 pushbuttons can be assigned to one receiver unit - Each receiver has 8 transistor outputs (one-shot operation) - A pushbutton can be assigned to multiple outputs of a receiver - Wireless communication is confirmed with a colored LED indicator on the pushbuttons - 922.5MHz frequency band reduces interference, providing a better signal in locations with obstacles - A high-sensitivity magnetic-base antenna is an option when installing the receiver inside a control panel

    04:08

Onlinecomponents.com features Omron’s wireless buttons

September 02, 2019 Onlinecomponents.com features Omron’s wireless buttons talking about how we've made wireless communication in industrial settings extremely easy.
READ MORE
corporate
The visit of the chancellor of Germany, Angela Merkel at Omron at Hannover Messe
  • The visit of the chancellor of Germany, Angela Merkel at Omron at Hannover Messe

    The visit of the chancellor of Germany, Angela Merkel at Omron at Hannover Messe

    The Omron team was honoured to welcome the Chancellor of Germany, Angela Merkel, together with Stefan Löfven, the Prime Minister of Sweden, at our booth at Hannover Messe yesterday! ------- We demonstrated how #artificialintelligence, smart robotics, as well as advanced sensor and control technologies can change manufacturing, where humans and machines work in close cooperation to complement each other. ------ Linkedin post: SUBSCRIBE to our channel for more!

    00:51

Hannover Messe: Chancellor Merkel impressed by harmonious interaction of man and machine

April 04, 2019 German Chancellor and Swedish Prime Minister meet AI-controlled table tennis robot FORPHEUS integrated with latest sensor and control technologies.
READ MORE
corporate
innovation-lab-stuttgart fcard event

Eight Innovation Labs offer 'proof of concept' to customers

October 19, 2018 We are proud to open the doors of eight new Innovation Labs in Europe. These labs enable manufacturers to experience the benefits of having a connected, automated and intelligent factory, optimized with the latest automation and robotics technologies, in addition to proof of concept testing for new environments.
READ MORE
corporate
ŠKODA AUTO uses Omron's fully autonomous LD mobile robot at Vrchlabí plant

ŠKODA AUTO uses LD mobile robot at Vrchlabí plant

September 27, 2018 The autonomous robot contributes to the continuous improvement of work safety in Vrchlabí and helps to minimise work risks. It recognises people crossing its path as well as other vehicles and stationary obstacles.
READ MORE