Latest news
Increased precision: Robert Bosch GmbH chooses new OMRON inline 3D CT X-ray inspection system VT-X750
04 August, 2022 Printed circuit boards (PCBs) are central component of numerous electrical devices, and the automotive industry is also increasingly dependent on PCBs that do not have any weak points.
Updated notice about OMRON Business Operations in Russia
01 August, 2022 Since our decision on March 14th to suspend temporarily shipments into Russia and Ukraine for our industrial automation, healthcare, and electronic components businesses, we have been closely monitoring the situation in the region. After carefully examining the future sustainability of our local operations, we have decided that it is not feasible to continue our industrial automation and electronic components businesses in Russia.
OMRON Acquires Science Based Targets Initiative Certification
19 July, 2022 Based on the greenhouse gas (GHG) emissions reduction targets set in its long-term vision, Shaping the Future 2030 (SF2030), OMRON paves the way for achieving the goal of limiting global warming to 1.5 degrees Celsius advocated by the Paris Agreement.
OMRON Adds Selectable Autonomy and FLOW iQ to FLOW Core Fleet Management Software
11 July, 2022 Driving flexible manufacturing with mobile robots in complex material transport applications
Multiple vulnerabilities in Machine Automation Controller NJ/NX series
01 July, 2022 Information on the vulnerabilities that exist in the NJ/NX series.
OMRON’s Flexible Manufacturing Roadshow travels across Europe
08 June, 2022 Our Flexible Manufacturing Roadshow has embarked on a unique journey across Europe, featuring exclusive demonstrations of human-machine collaborative solutions not usually seen outside of a factory setting due to their size and scale.
OMRON launches K7TM condition monitoring device for predictive maintenance of heaters
28 April, 2022 OMRON's new K7TM condition monitor for heater equipment in automotive and FMCG industries contributes to the realization of a carbon-free society.
OMRON adds new food-grade models to its i4H SCARA lineup
20 April, 2022 OMRON introduces the additions of new food-grade robots to the i4H product line for safe handling in the food and beverage and packaging industry.
Update impact of Ukraine/Russia situation
15 April, 2022 OMRON has suspended shipments to Russia, Ukraine and Belarus until further notice.
OMRON announces “Shaping the Future 2030” vision
05 April, 2022 Targets 930 billion yen net sales and 120 billion yen operating income in the 1st phase (FY 2024)
OMRON brings real manufacturing evolution to factory floors today at Hannover Messe 2022
04 April, 2022 Automation beyond human abilities, advanced collaboration between people and machines and accelerating digital transformation at manufacturing sites will help manufacturers realize flexible, efficient, and sustainable production. Visit OMRON at Hannover Messe 2022 (30 May – 2 June) in hall 9, booth F24.
Discover career opportunities at OMRON
23 March, 2022 OMRON has recently launched a global career site, offering positions ranging from student programs to full-time positions worldwide.
Easy electrical wiring design for Omron panel solutions with PCSCHEMATIC
11 September, 2019 1500 Omron components to be included in the electrical CAD software PCSCHEMATIC Automation.
-
Component Focus: Omron Wireless Buttons
I'm Josh Bishop for cooling. It takes a wide voltage input from 100 to 240 volts AC and accepts either 50 or 60 Hertz. You can connect the incoming power here at the bottom with line, neutral and ground inputs. This particular power supply outputs the 24 volt DC power at the top with these terminal blocks and can provide up to 15 watts which is ample power for this wireless receiver or many other devices. There are other S8V caged power supplies that can output more power, but this works great in this case. The S8VK is providing power to this wireless receiver the A2W-RPC- WC1. This receiver is very straightforward to use with clearly marked ports and switches and common sense usage. This has eight outputs and accordingly can be synced with eight wireless buttons. You can see the power input up at the top and the outputs here at the bottom. There are lights for power, any potential errors and receipt of signals right here. There's also a slide switch for usage testing and setup. You'll note that this is 922.5 megahertz which gives it a greater range and better signal propagation than higher frequency signals. We end up with the communication assistance of about 100 meters without any obstructions. Finally we have the two push-button switches. They're obviously both wireless and they generate their own power so no battery is required. This also eliminates the need for maintenance. A light comes on when you click the button showing that it has been actuated and is working. They come with the space to allow you to easily mount them and swap them around as you need. The buttons are functionally the same, but you have the option of different types of plungers depending on what works best in your situation. They're both ULl certified, rated up to 1 million operations and are IP65 sealed. They're also shock and vibration resistant making them ideal for tough industrial application. All of this is connected and powered up. It is not set up and I'll walk you through the process just to show you how easy it is for you. You'll need to connect the S8VK to power. Again it can use power from practically anywhere in the world. Then hook the output of the power supply to the input of the wireless receiver and now everything will turn on and you'll be up to the point where I am currently. Programming the buttons and the receiver doesn't require anything external like a computer, you simply set the rotary switch to the channel you want to use, move the slide switch to ID and then click the button you want to use, 3 times relatively quickly. You'll see the receive light come on indicating that the receiver got the message and it has been paired. Switch to another channel do the same thing with the other button. That's it! It's recommended to make certain other systems in the area are not in use during this procedure, however, as it may cause problems. Let's move the slider switch to run and start clicking these buttons and watch those different indicators light up. Now deleting the buttons and reassigning them is just as easy; put the rotary switched to delete and click the button three times until the light comes on. The button is now unassigned and can be programmed to another output slot. With just a few components in a couple minutes of setup you can easily integrate Omron's wireless buttons into your systems. if you want to learn more or purchase these Omron components go to Features: - 8 pushbuttons can be assigned to one receiver unit - Each receiver has 8 transistor outputs (one-shot operation) - A pushbutton can be assigned to multiple outputs of a receiver - Wireless communication is confirmed with a colored LED indicator on the pushbuttons - 922.5MHz frequency band reduces interference, providing a better signal in locations with obstacles - A high-sensitivity magnetic-base antenna is an option when installing the receiver inside a control panel
04:08
Onlinecomponents.com features Omron’s wireless buttons
02 September, 2019 Onlinecomponents.com features Omron’s wireless buttons talking about how we've made wireless communication in industrial settings extremely easy.
Innovation in panel building: new terminal and solid-state relay models with Push-In Plus technology
13 August, 2019 Reduce your workload and save space in panel building - NEW G6D-F4PU Terminal Relay & G3DZ-F4PU Terminal SSR (solid-state relay) with Push-in Plus technology.
New Models of E2E NEXT Series Proximity Sensors
03 June, 2019 Sensors are equipped with IoT features to prevent stoppage and downtime.
New RX2-Series – The Driving Evolution
01 May, 2019 Versatile high-performance inverter helps maximize performance while saving energy.
New Sysmac AI Controller reduces downtime and extends equipment life
25 January, 2019 Artificial Intelligence solution collects, analyzes and utilizes data on ‘Edge’ devices within a controller to prolong equipment longevity and detects abnormalities to prevent failures.
-
Omron NX-Series Safety Network Controller
NX Series CIP Safety Controller with EtherCAT and Ethernet/IP capabilities. In addition to new hardware, Sysmac Studio new functions include Automatic Programming, Safety Data Logging, and Online Functional Test. For more information visit: USA Canada Mexico
03:16
New NX-Series Safety Network Controller
21 January, 2019 World's first* advanced safety controller to support two industrial safety networks for industrial robot systems
Ultimate flexibility to fit ever-changing production scene
12 November, 2018 OMRON introduces FHV7-series Smart Camera with World’s First Multi-color Light and 12 Megapixel Image Sensor
More profit for panel builders with G2RV-SR
03 September, 2018 By giving the humble relay a “starring role”
Even better than the human eye
27 August, 2018 Newly enhanced OMRON FH Series Vision System
New IoT Processing control sensors E8FC - Flow and E8PC - Pressure
23 August, 2018 New Flow sensors E8FC and Pressure sensors E8PC present the new generation of innovative solutions to control industrial process with different fluids and gases.
New MobilePlanner tablet Software
23 July, 2018 A new “lite” and easier-to-use version of our MobilePlanner for LD robots is now available. This means that customers can now have a centralised PC version for (re)configuration and robot management and a simpler version that can be used anywhere in the facility for routine interaction.
Omron brings the factory of the future to PPMA 2019
20 August, 2019 See our flexible production system on stand B36.
Seigo Kinugawa appointed as new CEO
14 May, 2019 Bringing a unique global perspective, Kinugawa will focus on responding to social needs with innovative manufacturing solutions.
Together we make the difference: Omron partners with Cembre in EMEA
08 April, 2019 The co-operation aims to meet the needs of panel builders, in terms of safety, consistency of control and simplification of maintenance
-
The visit of the chancellor of Germany, Angela Merkel at Omron at Hannover Messe #hm19
The Omron team was honoured to welcome the Chancellor of Germany, Angela Merkel, together with Stefan Löfven, the Prime Minister of Sweden, at our booth at Hannover Messe yesterday! ------- We demonstrated how #artificialintelligence, smart robotics, as well as advanced sensor and control technologies can change manufacturing, where humans and machines work in close cooperation to complement each other. ------ Linkedin post: SUBSCRIBE to our channel for more!
00:51
Hannover Messe: Chancellor Merkel impressed by harmonious interaction of man and machine
04 April, 2019 German Chancellor and Swedish Prime Minister meet AI-controlled table tennis robot FORPHEUS integrated with latest sensor and control technologies.
Making a business case for Artificial Intelligence
16 January, 2019 On Wednesday, December 5, around 100 professionals gathered in Malmö to attend an Omron conference about the use of artificial intelligence in the manufacturing industry.
Omron Hosts ASTM International Committee F45 Summit
18 December, 2018 The event aims to ensure productive deployment of innovative mobile robotics technology.
TM Series collaborative robots accelerate the harmonization of humans and machines
30 November, 2018 Omron has announced the global launch of the TM series collaborative robot family to realize an innovative manufacturing environment where humans and machines work in harmony.
Eight Innovation Labs offer 'proof of concept' to customers
19 October, 2018 OMRON - one of the world´s leading suppliers of industrial automation– is proud to open the doors of eight new Innovation Labs in Europe.
-
ŠKODA AUTO uses Omron's fully autonomous LD mobile robot at Vrchlabí plant
The autonomous robot contributes to the continuous improvement of work safety in Vrchlabí and helps to minimise work risks. It recognises people crossing its path as well as other vehicles and stationary obstacles.
03:00
ŠKODA AUTO uses LD mobile robot at Vrchlabí plant
27 September, 2018 The autonomous robot contributes to the continuous improvement of work safety in Vrchlabí and helps to minimise work risks. It recognises people crossing its path as well as other vehicles and stationary obstacles.
Ensure product quality, compliance and consumer safety
23 August, 2018 Acquisition of Microscan Systems brings in 35+ years of barcode reading, machine vision and verification expertise
Omron Enters Distribution Agreement with Electro Performance
26 July, 2018 Electro Performance Offers Full Technical Service and Installation at Customer Sites in Denmark