Agile and clever tailor-made mobile robotics
Published on 2019-11-04 09:57:27 UTC in Collaborative Robotics
Revolutionizing human-machine collaboration in the automotive industry.
Major German automotive group optimizes efficiency and innovation leadership in material handling with Omron LD mobile robots and a conveyor attachment from cts GmbH.
Automobile production and assembly line production have always been closely linked. It was not until Henry Ford began using conveyor belts in his factories in 1913 that the car was able to conquer the world as a mass-produced product. Today, a working day without assembly lines is inconceivable at the BMW factories. The group relies on innovative transport and logistics to increase efficiency and flexibility, to better link work processes, as well as to relieve employees from repetitive and time-consuming tasks. These concepts include Omron LD mobile robots for material transport that deliver a particularly high return on investment (ROI). These autonomous mobile robots are equipped with a conveyor tower - a height-adjustable load handling device, developed by system integrator cts GmbH. The interaction between employees and transport robots at BMW impressively demonstrates how factory harmony can be implemented in the factory of the future.
Goal: Continuous optimization of production and logistics processes
Depending on the BMW plant, up to 1600 vehicles are produced each day. With such production volumes, continuous optimization and efficiency gains through innovative strategies and technologies are essential. This also includes logistics and transport processes in production. Various small and large parts, including components for steering wheel and cockpit assembly, rotable parts or interior lights for example, must be transported continuously from storage to the assembly line.
"Employees in the production halls were involved in the transport of components for more than 60 percent of their working time. Merging the different storage and production areas with conveyor belts is impractical, so this step was mostly done manually, which cost valuable capacity," says Aleksandar Cvetanovic, European Key Account Manager, Automotive at Omron Industrial Automation Europe.
Mini Smart Transporters address needs and requirements
BMW factories have utilized an automated and driverless transport system since the 1980s. However, this system is not flexible in its use and is tied to fixed routes via lanes in the form of grooves. BMW needed a robot that could transport the so-called small load carriers (SLC/KLT), to create its own route. This transport robot needed to be able to flexibly and quickly adapt to new processes without having to make major changes to the infrastructure - an advantage over line-guided materials handling.Ideal route determined independently
Since 2015, the BMW Group has developed the first self-driving Smart Transport Robots (STR), together with the Fraunhofer Institute IML, for the transport of roll containers on logistics areas within production halls. The second generation is now in operation at the BMW Group Regensburg plant. The robots carry roll containers weighing up to one ton and transport them autonomously to the destination of the goods. They calculate the ideal route independently and move freely in the area. The new navigation method SLAM (Simultaneous Localization and Mapping) does not require any permanently installed navigation transmitters in buildings and thus can be used quickly in a new environment. A built-in battery module of the BMW i3 powers the STR for a whole working shift. The delivery of urgent small parts is handled by a smaller version of the STR - the miniSTR based on the Omron LD mobile robot.Omron convinces with worldwide service and support
"To fully automate the intralogistics and bring manufacturing automation together with Industry 4.0 and digitization, a solution for material transfer had to be developed using the software architecture from the cts middleware AIV-Framework," says Cvetanovic. "Our Enterprise Manager fleet management system has more options than other vendor solutions. The narrow and high design of the solution was also beneficial, as there are quite narrow paths and high equipment in use at the BMW plant. However, the main reason that BMW has opted for Omron was the global service and support. More than a good technical solution alone is needed for a global company like BMW.”Our mobile robots were first implemented at the Landshut plant, with other production sites such as Munich, Wackersdorf, Berlin, Leipzig, Regensburg, Eisenach and Dingolfing currently being implemented.
Contact us for more information