Login

We are experiencing technical difficulties. Your form submission has not been successful. Please accept our apologies and try again later. Details: [details]

Register

We are experiencing technical difficulties. Your form submission has not been successful. Please accept our apologies and try again later. Details: [details]
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
We are experiencing technical difficulties. Your form submission has not been successful. Please accept our apologies and try again later. Details: [details]

Thank you for your interest

You now have access to From manual functional safety checks to guided testing: Modernising safety verification

A confirmation email has been sent to

Continue to page

Please or get direct access to download this document

Flexible Manufacturing
Operational Excellence
automation blog

From manual functional safety checks to guided testing: Modernising safety verification

Published on 06 May, 2025 in Flexible Manufacturing

From manual funtional safety checks to guided testing: Modernising safety verification

Functional safety is fundamental to every industrial automation system. From emergency stop buttons to interlocks and light curtains, the role of safety components and its safety chain is to protect people and to ensure machine integrity and regulatory compliance. Yet verifying that these systems work correctly, especially during commissioning and maintenance for the entire lifetime of machinery, remains a complex and time-consuming task with high costs in many factories.

Traditional safety verification: Manual, repetitive, and labour-intensive

Traditionally, safety verification involves at least a team of engineers. One remains at the control panel or operating station, monitoring feedback from the system screen. The other walks the machinery line, pressing buttons and activating devices on command. They must coordinate each test verbally or by signs: “Ready?”, “Pressed”, “OK—release”, and so on. The results are usually noted down manually and, in some cases, only partially documented and many important details may be missed after some working hours. This manual process is repeated across every safety device and every machine cell—resulting in an enormous workload, especially in larger installations and well as potential machine downtime.

A smarter approach: Online Safety Functional Test Verification in Sysmac Studio

OMRON’s NX Safety platform introduces a more efficient and reliable way to verify safety functions through a feature called Online Safety Functional Test Verification. Integrated into the Sysmac Studio software, this tool enables operators to validate safety  (Input-Logic-Output safety chain) logic and device responses directly on live systems—without needing to script tests manually or rely on coordination between multiple persons.

The concept is simple: connect a PC to the NX Safety Controller, either via Ethernet or wirelessly, and open the Online Functional Test tool within Sysmac Studio. The software guides the user through each action and verification step, prompting the operator to activate specific safety components in sequence. As each action is performed—such as pressing an emergency stop or breaking a light curtain beam—the tool captures the corresponding response from the safety program and logs it, complete with timestamps. Results are displayed in real time and can be reviewed on the spot.

Clear reporting and digital traceability

Once all steps are completed, the software generates a test report, including a safety signature. Regularly, this signature also appears on the controller’s seven-segment display, providing a simple visual confirmation that the system has the same verified program. Reports can be exported and archived, creating a reliable audit trail for safety certification or future inspections.

The tool also supports re-testing of failed steps, annotation of observations, and repeat testing after modifications—making it a practical solution for both initial commissioning and ongoing maintenance activities. Because the system records each interaction digitally, it improves traceability and supports compliance with relevant international standards, including IEC 61508 (SIL3) and ISO 13849-1 (PLe).

Fewer resources, greater confidence

One of the major advantages of the Online Safety Functional Test is that it reduces the number of skilled personnel required during verification on site. In many cases, a single operator can complete the entire test cycle, just following the on-screen instructions and interacting with physical components without needing a second or many persons to monitor the system remotely. This not only saves time but also helps standardise procedures across teams, shifts, or sites.

OMRON’s NX Safety platform offers a complete solution for modular, scalable, and standards-compliant safety control. The Online Safety Functional Test Verification feature brings a valuable tool to engineering teams seeking to reduce risk, streamline verification, and improve documentation, whilst maintaining full control over system safety.

Contact us for more information

Online Safety Functional Test: From manual functional safety checks to guided testing

From manual functional safety checks to guided testing: Modernising safety verification. Online Safety Functional Test reduces the number of skilled personnel required during verification on site.

  • 2:13 -   From manual functional safety checks to guided testing: Modernising safety verification. Online Safety Functional Test reduces the number of skilled personnel required during verification on site.

Contact Omron specialists

Do you have any questions or would you like personal advice? Feel free to contact one of our specialists.
  • Omron Europe

    Omron Europe