Login

We are experiencing technical difficulties. Your form submission has not been successful. Please accept our apologies and try again later. Details: [details]

Register

We are experiencing technical difficulties. Your form submission has not been successful. Please accept our apologies and try again later. Details: [details]
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
We are experiencing technical difficulties. Your form submission has not been successful. Please accept our apologies and try again later. Details: [details]

Thank you for your interest

You now have access to Customised machines: Modular design in an integrated environment

A confirmation email has been sent to

Continue to page

Please or register to download this document

Flexible Manufacturing

Customised Machines: Modular design in an integrated environment

Published on 02 September, 2025 in Flexible Manufacturing

How to configure and personalise machine functionality at runtime

In today’s fast-paced industrial landscape, the demand for customised machines is on the rise. Machine builders face the challenge of producing unique machines tailored to specific customer requirements. Due to the many variations, this leads to inefficiencies in development, commissioning, and maintenance. OMRON’s Integrated Development Environment (IDE) Sysmac Studio offers a solution that streamlines the machine development process. An environment that stimulates the creativity and full potential of programmers.

The problem: Every machine is a new project

Let’s face it: no matter how many machines of type X or Y you produce each year, almost every delivery becomes a custom job. Customers demand changes in layout, speed, materials, safety functionality, or product handling. As a result, machine builders face the recurring challenge of:
  • Redundant engineering efforts
  • Longer commissioning times
  • Higher risks of errors and after-sales issues
  • Increased costs and delays
The struggle to manage these variations is a daily pain point for technical managers, who must navigate the intricacies of machine customization while contending with a shortage of skilled labor. To combat these issues, many builders are turning to innovative tools that can significantly reduce engineering time and enhance efficiency.

The ultimate dream of a machine builder

Imagine a world where the entire machine development process — from initial customer request to final commissioning — is fully integrated and largely automated. This is the ultimate aspiration for many machine builders to automate all repetitive engineering steps between a request for quotation (RFQ) and site acceptance test (SAT):
  • Based on the RFQ, dynamically configure machine functionalities with automated feasibility checks
  • Instantly visualise and validate the design with the customer through simulation: "Is this what you had in mind?"
  • Use a digital twin to simulate machine performance across different scenarios provided
  • Automatically generate accurate quotations for labour and materials
  • Directly link CAD designs to machine code generation
  • Produce complete documentation packages, from manuals to maintenance schedules, without extra effort
It’s a vision that would transform efficiency, responsiveness, and cost control across the entire lifecycle of customised machines.

The path forward: What machine builders are doing today

To move toward that goal, machine builders are already laying the groundwork with smarter engineering practices today:
  • Adopting modular design principles to allow scalable, flexible machine configurations that can evolve with customer demands
  • Developing pre-engineered lines and modular systems that can be assembled on demand
  • Applying modularity not just to hardware (mechanical/electrical), but to control software as well, enabling faster re-use and adaptation
These are important steps, but they still require a supportive technical ecosystem to be fully effective.

Enabling the vision: OMRON helps to make it real

This is where OMRON’s Sysmac platform and development tools offer real value by turning that vision into tangible progress:
  • One software source for machine control: A unified user-friendly interface for: PLC, motion, human-machine interface (HMI), safety, robotics control, all in one download.
  • 3D simulation of the machine movements: This allows engineers to visualize machine operations in a virtual environment, ensuring accurate testing and validation before physical implementation.
  • During commissioning the Sysmac platform offers one project to be able to effectively personalize machines per customer, including safety!
  • Scalability: The platform can grow with the needs of the customer, accommodating new functionalities and configurations as required, or scale down and ‘downtune’ when options are not needed and a basic machine fits the requirement.

How: Streamlining development and commissioning with OMRON’s Sysmac platform

Unlike traditional tools that require multiple software packages and expert knowledge for different parts of a machine, Sysmac Studio simplifies everything:
  • A single software source for the entire control system
  • Built-in 3D motion simulation to visualize axis movement, robot kinematics, and full sequences
  • Wizard-based tools for project generation and machine setup
  • Easy connection to third-party design environments like ePlan, Matlab/Simulink, Solidworks, Flowsource or AutomationML
  • Configuration instead of programming – especially powerful during Factory Acceptance Testing (FAT) or Site Acceptance Testing (SAT)

EtherCAT Extended Functions: The enabler of modular machines

Modularity isn’t just a mechanical concept. It applies to control software and communication as well. OMRON’s EtherCAT Extended Functions (EEF v3) redefine how we approach the design and implementation of modular machines. They go beyond standard network communication. Automatic detection and mapping of the EtherCAT I/O and motion devices, and with that exact functionality present in the machine — plus integrity of hardware troubleshooting — facilitates scalable machine sections with plug-and-play EtherCAT nodes. As a result, it allows machine builders to maintain a single project template and configure specific machine options at runtime.

Operational benefits for customers

The advantages of OMRON’s approach extend beyond just faster development times. Customers also benefit from:
  • Customizable machines: Technology such as OMRON’s EtherCAT Extended Functions facilitates easy machine module selection, allowing for customisation without altering the underlying program.
  • Simplified troubleshooting: Maintenance becomes more straightforward with user-friendly interfaces, enabling quick adjustments and updates.
  • Increased flexibility: The ability to load new controller programs, even without the need for proprietary software tools, enhances operational efficiency on site.
  • And with the various focused features in a single software platform, machines can be commissioned in half the time compared to traditional approaches. 

Conclusion: OMRON’s Commitment to Innovation

OMRON empowers machine builders to turn complexity into competitive advantage. With our integrated Sysmac platform and engineering tools, building customised machines is no longer a challenge, it’s a strategic asset.
 
Discover OMRON’s Sysmac platform
Contact us for more information

Contact Omron specialists

Do you have any questions or would you like personal advice? Feel free to contact one of our specialists.
  • Omron Europe

    Omron Europe