Optimal lineside replenishment is key to improve your Overall Equipment Effectiveness (OEE):
- To avoid waiting time for machines
- To eliminate intermediate stock
But also: the manual operations to perform these tasks are not ergonomic and can create safety issues for operators.
Our efforts improve Line Side Replenishment (LSR), while eliminating line starvation and mistakes, and avoid operators having to perform these repetitive tasks.
Our Solution: Cobots for Material Feeding
OMRON offers a wide array of robotic solutions, not only improving throughput, but freeing workers to concentrate on value-add tasks.
Collaborative robots for material feeding.
The Cobot picks packaging consumables as cartons from one position and places them directly onto the conveyor or in the packaging machine. This reduces or even eliminates the need to manually unload these consumables.
Other examples are Selective Compliance Assembly Robot Arms (SCARA) solutions that are tasked with loading bottles or other containers or high speed parallel robotic solutions used to orientate and align-items.
Benefits of an Automated Consumables Supply
- Avoids costly and time-consuming line starvation.
- Improves production consistency & output.
- Avoids repetitive tasks and reduces worker stress.
- Allows verification of the correct package and product combination through traceability.
See the Solution in Action

-
OMRON TM Collaborative robots working alongside employees to boost the capabilities of manufacturing
See how a manufacturer of plastic containers achieves major boost in flexibility and customer satisfaction with Omron TM collaborative robot. Visit Omron Automation and read complete success story Visit system integrator partner Sure Controls Visit end user Schoeneck Containers, Inc. (SCI) Schoeneck Containers, Inc. (SCI), a family-owned, family-operated company based in Wisconsin that manufactures plastic containers for diverse consumer and commercial markets throughout the world, began considering a collaborative robotic solution to keep up with production demands in the face of a severe labor shortage. This solution would involve robotic technologies working alongside employees to augment the capabilities of SCI’s team. With the help of a Wisconsin industrial equipment distributor and system integrator named Sure Controls. SCI was able to get the robot up and running in a single day, and the team quickly saw major improvements in customer satisfaction as well as a significant boost in overall production flexibility. #Robotics #FlexibleManufacturing #Packaging #manufacturing #OmronAutomation #CollaborativeRobot
05:09
OMRON TM Collaborative robots working alongside employees to boost the capabilities of manufacturing
See how a manufacturer of plastic containers achieves major boost in flexibility and customer satisfaction with Omron TM collaborative robot. Visit Omron Automation and read complete success story Visit system integrator partner Sure Controls Visit end user Schoeneck Containers, Inc. (SCI) Schoeneck Containers, Inc. (SCI), a family-owned, family-operated company based in Wisconsin that manufactures plastic containers for diverse consumer and commercial markets throughout the world, began considering a collaborative robotic solution to keep up with production demands in the face of a severe labor shortage. This solution would involve robotic technologies working alongside employees to augment the capabilities of SCI’s team. With the help of a Wisconsin industrial equipment distributor and system integrator named Sure Controls. SCI was able to get the robot up and running in a single day, and the team quickly saw major improvements in customer satisfaction as well as a significant boost in overall production flexibility. #Robotics #FlexibleManufacturing #Packaging #manufacturing #OmronAutomation #CollaborativeRobot
-
Robotic Unscrambler
POSIMAT has developed the POSIROBOT, its unique solution for robotic unscramblers. Its main features are: • 115 bot/min with a single robot • Bottle transfer system high efficiency & simplicity • Multiformat handles any shape and dimensions • Gentle handling of bottles through the entire process • 360º bottle orientator • Puck line compatible
01:17
Robotic Unscrambler
POSIMAT has developed the POSIROBOT, its unique solution for robotic unscramblers. Its main features are: • 115 bot/min with a single robot • Bottle transfer system high efficiency & simplicity • Multiformat handles any shape and dimensions • Gentle handling of bottles through the entire process • 360º bottle orientator • Puck line compatibleRelated Products
See also our other Key Applications & Solutions

Mixed Boxes in Secondary Packaging
To handle & optimize the inflow of different goods, we bring together a complete line of robotic automation products into a single, fully integrated packaging system.

Intralogistics & Intermediate Stocks
Our wide array of smart robotic solutions optimizes the throughput and availability of goods needed.

Unpacking and Distribution of Arriving Goods
Together with our partners OMRON can address unpacking and distribution of arriving goods issues and realize fully automated handling & movement of these goods.

End-of-Line Palletizing
Together with our partners we realize smart and efficient EOL-palletizing solutions.