Login

We are experiencing technical difficulties. Your form submission has not been successful. Please accept our apologies and try again later. Details: [details]

Register

We are experiencing technical difficulties. Your form submission has not been successful. Please accept our apologies and try again later. Details: [details]
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
We are experiencing technical difficulties. Your form submission has not been successful. Please accept our apologies and try again later. Details: [details]

Thank you for your interest

You now have access to ŠKODA AUTO uses LD mobile robot at Vrchlabí plant

A confirmation email has been sent to

Continue to page

Please or get direct access to download this document

Flexible Manufacturing
Sustainable Manufacturing
Applications

ŠKODA AUTO uses LD mobile robot at Vrchlabí plant

Published on 17 March, 2020 in Flexible Manufacturing

The autonomous robot contributes to the continuous improvement of work safety in Vrchlabí and helps to minimise work risks. It recognises people crossing its path as well as other vehicles and stationary obstacles.
  • A fully autonomous transport system carries parts between the mechanical measuring centre and processing machines
  • A guided tour is all the robot needs to grasp its route and environment
The Czech car manufacturer is using our fully autonomous, self-learning transport robot at their Vrchlabí component plant. This robot is able to recognise obstacles along its journey through the plant and to incorporate other information from its surroundings when planning its route. If necessary, it changes its course to always get to its destination as quickly as possible. It thereby contributes to further improving safety at work and the efficiency of transport processes at the plant.
On one trip, the transport robot can carry a load of up to 130 kg and chooses the correct paths fully autonomously. Unlike traditional automated transport systems, it does not require lane guidance in the form of induction loops, magnetic strips or reflectors. To learn the route, the vehicle only needs to be guided between the stations once via a tablet or joystick. In doing so, it captures its environment as well as changes to its surroundings all by itself and adapts its route if necessary.
Sophisticated, state-of-the-art technology enables the robot to navigate its environment: using sensors and laser scanners, it recognises vehicles and stationary obstacles as well as people crossing its path. The control system calculates the approach speed and detects if a collision is imminent. In this case, the robot stops by itself or takes evasive action. Unlike other systems used at ŠKODA AUTO, it immediately adjusts its route based on information from its surroundings, without having to stop in the process. If the fully autonomous robot detects that it will regularly encounter obstacles at a specific point along its journey, it changes its route permanently. If necessary, the electrically powered system is able to travel to all of the destinations at the Vrchlabí plant, which covers 16,000 m2.
The robot (tcm:40-80433) completes 120 trips per day and travels a total distance of 35 km on its route between the mechanical measuring centre and the processing machines. The testing and pilot phases have already been completed; the robot is in regular use at the factory starting from June 2018.
The increasing production numbers at ŠKODA AUTO translate into higher utilised capacity for the plants and more traffic in the production areas. The autonomous robot contributes to the continuous improvement of work safety in Vrchlabí and helps to minimise work risks.
In production, ŠKODA AUTO is systematically turning to technology from Industry 4.0, such as cooperating robots. These are used in the production of direct-shift transmissions at the Vrchlabí plant and support the employees with one of the most sensitive tasks in transmission production –inserting the gear actuator piston. A handling robot also supplies dozens of machines with parts and returns empty containers to the warehouse. The extensive ‘transparent factory’ IT system also forms part of operations. Contact us for more information

ŠKODA AUTO uses Omron's fully autonomous LD mobile robot at Vrchlabí plant

Contact Omron specialists

Do you have any questions or would you like personal advice? Feel free to contact one of our specialists.
  • Omron Europe

    Omron Europe