Login

We are experiencing technical difficulties. Your form submission has not been successful. Please accept our apologies and try again later. Details: [details]

Register

We are experiencing technical difficulties. Your form submission has not been successful. Please accept our apologies and try again later. Details: [details]
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
We are experiencing technical difficulties. Your form submission has not been successful. Please accept our apologies and try again later. Details: [details]

Thank you for your interest

You now have access to Automated pipetting solution ensures rapid evaluation of Covid-19 samples

A confirmation email has been sent to

Continue to page

Please or get direct access to download this document

With the continuing changes seen within the Covid-19 virus strains, it’s vital that any samples can be analysed as rapidly as possible. Two Bavarian companies, GriPS Automation GmbH and D&T engineering GmbH, have worked together with OMRON to streamline the pipetting part of the process, reducing processing time from one hour to ten minutes per plate.

As a result, the three companies have developed the PT600 laboratory processing system for the transfer of samples, using an OMRON Cobra 450 robot for contactless transport. The new solution was developed because the testing of standard Covid-19 samples requires removing a measured sample of the liquid and transferring it to a tube in which it can be properly tested. To do this task manually is time-intensive and can also introduce a level of human error. The automation of the pipetting process is designed to eliminate such errors.

  • 0:00 -   Automated pipetting solution ensures rapid evaluation of Covid-19 samples

The OMRON Cobra 450 is a four-axis Scara robot with a reach of 450mm. Designed for processes such as material handling, assembly and precision machining, it offers excellent repeatability. This particular project requires the sample to be pipetted into a ‘deep well’ plate, with 96 compartments. A tip has to be placed on the pipette, which is then used to draw a sample. A measured amount of this is then transferred into one of the compartments in the plate. The process is repeated for the other 95 compartments.

grips pipetting a fcard sol

A complete, smart solution

The solution, that included the industrial robot, as well as a MicroHAWK V330-F compact barcode reader, highly precise G5 Series servo actuator, Gigabit Ethernet Vision Cameras and an industrial panel PC NYP35, automates the entire process, including the reading of the QR codes on the original tubes of liquid, and allocating each sample to the correct compartment. It eliminates any mistakes that can happen when this process is carried out manually. The speed of the automated operation is also much faster than the manual process. The latter can take up to an hour to fill a complete plate of 96 samples, whereas the robot can complete the task within ten minutes. It therefore saves a significant amount of time. The whole solution is controlled by our Sysmac platform and the NX1 controller is continuously updating the database with the barcode information of the samples via OPC-UA.

grips pipetting b fcard sol

The development of the new processing system started in December 2020 and was completed by May 2021. Guido Grimberg, CEO of GriPS Automation, says: “The first fully automated PT600 machine is now being used in a laboratory and everything works perfectly.”

He continues: “We’ve been working closely with OMRON for 25 years now, and we’ve developed a lot of system integrations together. They were therefore a natural choice for automating this solution. OMRON offers a very wide product range, which has supported us in developing the overall solution. From the displays to robots, barcode readers, drive technology, and the control system etc. This simplifies our life, as one company can deliver a total, smart solution.”

Guido Grimberg adds: “Industry 4.0 is a key topic at the moment. This project involved issues such as the pandemic, traceability and the need to collect and analyse reliable data. This is a passion for us, which is why we were involved in developing the PT600.”

Contact us for more information

Related products

  • omnucg5-moter prod

    At the heart of every great machine

  • NX1 prod

    Information & Productivity in a miniaturized size controller

  • industrial-15 inch hmi+ipc-01-4b prod

    Industrial Panel PC

  • FV 330-F left small  side en prod

    MicroHAWK V330-F Multicode Reader