Login

We are experiencing technical difficulties. Your form submission has not been successful. Please accept our apologies and try again later. Details: [details]

Register

We are experiencing technical difficulties. Your form submission has not been successful. Please accept our apologies and try again later. Details: [details]
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
We are experiencing technical difficulties. Your form submission has not been successful. Please accept our apologies and try again later. Details: [details]

Thank you for your interest

You now have access to Vadain automates the inspection of curtain fabrics with machine vision

A confirmation email has been sent to

Continue to page

Please or get direct access to download this document

Brand Protection
news

Vadain automates the inspection of curtain fabrics with machine vision

Published on 08 April, 2022 in Brand Protection

Vadain, the market leader in custom curtains in the Netherlands, needed a solution to detect errors as early as possible in kilometers of curtain fabrics. Together with software developers from Sycade, OMRON machine vision technology, and machine builder Eisenkolb, they developed an automated solution to detect and analyze errors in curtain fabrics, making the time-consuming manual inspection process a thing of the past.

The challenge: Flawless curtains

Delivering flawless curtains is a top priority for Vadain. In addition to the right dimensions, correct production method and finishing, identifying and preventing fabric defects before they enter production is a crucial step. If any flaws are detected once the curtains are hung at the customer’s premises, they are very costly to remedy, including replacing the product, as well as all associated logistics processes and work hours.

Production defects

As a rule of thumb, Vadain estimates that an average roll of fabric may contain a maximum of 5 defects, such as weaving errors or stains. In the best case, a fabric supplier has already marked the flaws in the roll. However, the responsibility for detecting and processing the defects is passed on to Vadain.

Quality checks

To prevent any defects, several checks are made between the receipt of goods and dispatching the finished product. The first check takes place when the material arrives and is stored in the warehouse. More checks are carried out prior to production and at the workshop before production, as well as a final quality check of the finished product before shipment. The inspection was done manually, by unrolling and rolling the fabric over light boxes.
While rolling, an employee visually checks for errors in the fabric. With thousands of different types and tens of kilometers of fabric in stock, this is a very time-consuming and inefficient procedure. Also, an employee can only carry out these checks for a short time with full attention. As soon as the inspection is done and the fabric goes to production, the fabric is then cut to size on light boxes. Once again, the seamstress or cutter carries out a quality check. With their trained eyes, they rarely miss an error.

Solution with machine vision

The team at Vadain thought that there must be a better, more efficient and faster way to inspect the fabrics, and presented the challenge to Sycade, an expert in the field of quality improvement through automation in the manufacturing industry. Sycade proposed a concept to automate the inspection process with a machine vision solution. The solution performs checks faster and more accurately, reduces complaints and cutting loss* and ultimately results in cost savings. With the expertise of Vadain, the technology and innovative automation concept of OMRON, hardware of Eisenkolb and a camera light supplier, Sycade set up a solution using a 'standard' rolling machine to unroll rolls from position A and roll up again to position B. The unrolled fabric passes over an assessment surface with an integrated cutting unit, located inside a dark unit with vision technology.

Cutting loss*

Cutting loss occurs when rolls are cut for production. Residual pieces are regarded as cutting loss, and largely disposed of as waste. By accurately documenting fabric lengths on partial rolls—and matching these with the requirements for each order—cutting loss, waste and the associated costs can be minimized.  

Intelligent software

The lighting and camera inspection system can detect even the smallest deviations in substances, thanks to intelligent custom software from Sycade and 'customized' standard hardware from OMRON. However, it is not enough to simply find a fault in a roll of fabric. Fabrics are not all equally thick or transparent, and they come with different weave structures, colors and reflection. The correct light and camera adjustments and programming settings were discovered after a series of tests.

Detect, cut, register

What needs to be done when a defect is detected and assessed? In the case of dust, it can be removed by the operator and the machine receives a signal that it can pass. In the event of a stain or weaving error, the machine has already identified the location of the defect. The machine has also already measured how much fabric has been unrolled up to the defect. After cutting from the correct location, this partial roll is marked with a sticker with the parent roll plus partial roll marking, including the number of meters. This makes it possible to have an overview of how many meters of flawless fabric is in stock and in which cuts. This ensures that the workshop knows exactly which partial—and error free—roll can be used most efficiently for a particular order. In the administration, the total of the sub-rolls remains linked to the original meters of the parent roll, making it easy and efficient to reorder fabrics.

Collateral advantage

Thanks to the solution, pick-up and return movements in the warehouse have been halved. An unforeseen but welcome advantage. As the partial rolls are now all precisely measured, registered and pre-cut, complete rolls no longer need to be picked up, cut and returned to the warehouse. This saves 50% in the loading and unloading time. Reduced transport movements between the racks also improve safety.
Fate Basit, CEO of Sycade concludes: “In addition to tackling the initial problem, the solution has brought some very welcome additional benefits. We are convinced that our machine vision solution offers enormous opportunities for every organization in the manufacturing industry.”

Contact Omron specialists

Do you have any questions or would you like personal advice? Feel free to contact one of our specialists.
  • Omron Europe

    Omron Europe