Tray sealer with indexing flight bar drive system
Machine description
Empty trays are loaded by a tray denester on the infeed line and conveyed up to the sealing station. The sealing operation consists in welding a thermoplastic film on the edges of the trays, the operation being performed in a vacuum or in a neutral gas atmosphere. Before any sealing operation, a new length of film is unwound, positioned over the trays, welded on the edge of the trays and excess film wound again on a scrap roll.
Flight bar drive system
Trays are displaced over the entire length of the machine by a transport system provided with a series of transverse push bars which are equidistantly mounted between two lateral driving chains.
Machine main function groups
- Chain-Driven Indexer: Single conveyor comprising a series of transverse bars with two lateral driving chains.
- Sealing Station: Top bell-housing which contains 4 welding heads, bottom tank and bridge plates.
- Lifting System: The lower mould can be displaced upwardly by a pneumatic system.
- Film Feeding: A dancing arm system ensures the film tension control. A servo-driven pinch roller drives the film.
- Film Waste Rewinder: The skeleton of lidding material is re-wound onto a servo-driven mandrel.
A: Tray entry detection; B: Upper and lower limit positions of the dancing arm; C: Push-bar withdrawn position; D: Position of maximum advance; E: Differential pressure sensor
Your automation requirement - our complete solution
We are able to supply all the automation products for tray sealing machines, including the logic and motion or hybrid controller.
We can also provide all motors, drives, position sensors, safety devices, temperature sensors and other panel components. All are easy to integrate and carry the well-known Omron brand of quality and reliability.
Easy axis positioning
A position control card (CJ1W-NC[]81) is used to connect and control all the drives of the machine with built-in EtherCAT as motion bus. No need for complex wiring and individual parametrisation. All information is available through one access point, one program.
S-curve speed profile
The servo-drives (R88D-KN[]-ECT) speed profile can be programmed in the PLC with a standard PLCopen FB library in order to adapt, for example, the acceleration and deceleration of the push-bar according to the contents of the tray, in particular to avoid liquids slopping onto the seal area.
First-class temperature control for perfect seal
A 4-loop temperature control unit (CJ1W-TC002) regulates individually the temperature of 4 heater plates. The 2-PID control and the auto-tuning function enable each temperature control loop to provide answers with minimal overshoot at startup as well as give a good response to disturbance during production.
The result is a perfect seal right from the first tray which has an easy-peel film.
The right sensor for the right function
The wide range of Omron sensors allows you to detect transparent trays (E3X-SD), index flight bar position (HL-5000 / E3ZM) and detect the limit positions of the dancing arm (E3F2).
Related to this solution

Single-controller in a turnkey packaging line
The French specialist manufacturer of primary and secondary packaging machines recently developed a turnkey packaging line based on a single line controller.
More Automation Solutions

Packaging machine automation solutions
When you've been supplying automation solutions to packaging machine manufacturers for more than 20 years, you build quite a portfolio of different solutions and that’s exactly what we have done.