Sysmac Automation Platform

Sysmac is the latest machine automation platform from Omron with integration throughout: from controller to software.

The guiding principles behind the Sysmac automation platform are:
  • One control for the entire machine or production cell
  • Harmony between machine and people
  • Open communication and open programming standards.
The result: a powerful and robust automation platform with a new Machine Automation Controller, that integrates motion, sequencing, safety, networking and vision inspection, a new software (Sysmac Studio), that includes configuration, programming, simulation and monitoring and a fast machine network (EtherCAT) to control motion, safety, vision, sensors and actuators.

Sysmac Automation Platform

Since 1971 Sysmac has been used on PLCs, and has conveyed the Omron principles of reliability, robustness and fast control. Today we expand these principles across the whole machine.

Fastest Machine Network: To achieve the accuracy and predictability required by today’s machines, Omron selected EtherCAT, the fastest machine network. This is not only for motion, but IO, Safety and Vision. This gives a huge benefit to the customer simplifying the cabling and delivering astonishing performance.
Intel Architecture: Traditional ASIC based PLCs take time to develop and are not easy to change quickly. Sysmac uses an Intel® Atom™ or Core™ i7 processor and Real Time Operating System (RTOS) to shorten the development time and accelerate the ability to respond to new requirements. Performance can easily be scaled to suit the machine, without changing the design.
Sysmac_press_image_02.jpg
The scope of the Sysmac Platform from data to machine

Integrating motion, sequencing, vision and networks in ONE machine controller gives you complete control over the entire machine with high performance and easy operation.

Key Controller Features

  • EtherNet/IP and EtherCAT ports embedded
  • Standard IEC 61131-3 programming
  • Certified PLCopen Function Blocks for Motion Control
  • Global standards CE, cULus, NK, LR

Machine Control Features

  • Seamless integration of Logic and Motion
  • Synchronous control of all machine network devices
  • Backwards compatibility with most CJ PLC-series modules

Motion Control Features

  • Control up to 256 axes of motion
  • Linear and circular interpolation
  • Electronic cam and gearing

EtherCAT is the fastest emerging network for machine automation. It’s fast, accurate and highly efficient for the total machine.

Key EtherCAT features

  • Industrial Ethernet using standard IEEE 802.3 frames
  • High synchronization accuracy by using a distributed clock mechanism
  • The fastest network on the market with 100 μs refresh time and less than 1 μs jitter
  • Simple to set up with automatic address assignment for nodes
  • Uses standard Ethernet cables and connectors
  • Flexible Network Topology
  • On-the-Fly data exchange with slave devices for high throughput
  • Supports up to 512 slaves
  • Control Omron Servos, Inverters, Vision Systems, Robots, Distributed I/O, Safety, Sensors and more

One connection via the machine controller allows seamless control and communication with both the machine and the factory.
The Sysmac machine controllers join the world standard factory automation network, EtherNet/IP, with the best Ethernet-based machine control network, EtherCAT.

Key Ethernet/IP Features

  • Peer-to-Peer controller communication
  • Interface with NA HMI series or SCADA software
  • Database connection for MS SQL Server, Oracle, MySQL, IBM DB2 and Firebird
  • FTP
  • Support MATLAB/Simulink simulation software

One software to control and configure the entire machine via a single connection gives you the power and efficiency to develop and create like never before.

Learn it once
  • One software for logic, motion, safety, drives, vision and HMI
  • Fully compliant with the open standard IEC 61131-3
  • One consistent design environment
Develop it fast
  • Supports Ladder, Structured Text and Function Block programming with a comprehensive instruction set
  • Graphical CAM editor for easy development and programming of complex motion profiles
  • Intuitive editor with auto-complete assistance for Ladder and Structured Text programming
Test it as one
  • One simulation tool for sequence and motion in a 3D environment
  • Complete or partial program can be simulated and debugged
  • Data trending for tuning and debugging
  • Emulation of all Sysmac controllers functions
Secure it all
  • Advanced security function with 32 digit security password
  • Complete project or single Function Block can be protected (available in Sysmac Studio above v1.)
  • Machine cloning prevention
  • One Intuitive Interface

Applications

What our customers think

  • Kusatsu Factory Improves Productivity Based on Objective Data

    Omron Kusatsu factory adopted an easy-to-use solution that enables real-time tracing of a product through all the manufacturing processes, and provides visualization to analyze where improvements can be made. Learn more

    Machine controller achieves two-way database communication

    International print system manufacturer Ricoh is set to create links between its UK toner cartridge production and refill operations and a factory-level database, using Omron control technology to allow two-way real-time communications for the first time. Learn more
  • From wood to window frames in 60 seconds

    Thanks to our Sysmac platform, Working Process S.r.l., located in Niviano of Rivergaro, a few kilometers from Piacenza in Italy, achieved the goal of revolutionising the methodology of machining wooden frames, using a single automated line, and all completed in accordance with the relevant safety standards. Learn more

    Omron control powers die-cutting versatility in food & beverage

    “With our new DF350SR system, label converters handling short and long runs can switch between semi-rotary and full rotary mode, with a changeover time of only 10 minutes. By using Omron’s NJ controller, we have produced a powerful and flexible piece of kit, which effectively works as several machines in one.”  Daco Solutions Managing Director Dave Beynon Learn more
  • Roll grinding made easy [video]

    A control system based on products from Omron is helping machine-tool expert Halifax Numerical Controls (HNC) to achieve success in the UK and around the world in the fiercely competitive market for roll grinders for rubber-coated rollers. Learn more

Related products

  • 200W_Motor_R.png

    1S

    Simplified machine design and maintenance

  • Servo_drive_1_R.png

    1S

    Sysmac general purpose servo

  • R88L-EC-FW.jpg

    Accurax FW

    New Linear Motors with optimised efficiency

  • Accurax G5 drive_NEW.jpg

    Accurax G5

    At the heart of every great machine

  • omnucG5-moter.jpg

    Accurax G5

    At the heart of every great machine

  • R88L-EC-GW.jpg

    Accurax GW

    New Linear Motors with optimised efficiency

  • R88L-EA-AF.jpg

    Linear Axis (Cartesian) - Accurax

    Advanced Linear Motor Axis

  • Washdown Delta robot.jpg

    X-Delta

    The fastest picking system integrated in the Sysmac platform

  • FQ-M.jpg

    FQ-M

    Vision sensors for pick and place applications

  • Integrated_serv_ motor_1.jpg

    Integrated servo motor

    Motor and drive integrated for space optimization

  • MX2_nieuw.jpg

    MX2

    Born to Drive Machines

  • NA.jpg

    NA series

    The next generation of Machine Interface

  • NJ controller.jpg

    NJ series

    Sysmac controller - NJ series

  • NJ controller.jpg

    NJ1

    Sysmac controller – NJ1 Series

  • NJ controller.jpg

    NJ3

    Sysmac controller – NJ3 Series

  • NJ controller.jpg

    NJ5

    Sysmac controller – NJ5 Series

  • NX_Safety_FSoE_log0.jpg

    NX Safety distributed

    Integrated safety into machine automation

  • NX_Safety_product_Press_white.jpg

    NX-Safety stand alone

    NX Stand-alone Safety Controller

  • NX.jpg

    NX Series

    Performance and practicality for machine control

  • NX7_L.jpg

    NX7

    Sysmac controller – NX7 Series

  • RX-A4004_EF_right_FC_100_5000Hz_omron.jpg

    RX

    Customised to your machine

  • Sysmac Studio.jpg

    Sysmac Studio

    True Integrated Development Environment

Related product news

NX7_373x140.jpg

Introducing the new NJ1 and NX7 machine automation controllers

By introducing our new NJ1 and NX7 machine controllers, we have further expanded the lineup of Machine Automation Controllers which are at the heart of the Sysmac automation platform.
Learn more
NA.jpg

The new NA machine interface is bringing technology to life!

Designed following careful analysis of real applications and customer requirements, the new NA machine interface makes it fast and easy to implement dynamic, intuitive user interfaces that help boost productivity and minimise downtime by giving detailed real-time and historical insights into machine operation.
Learn more
OEE_EU_NX_Safety_Control_373x140.jpg

NX Safety Control: Next step towards the full integration of automation disciplines

The release of NX Safety Controller, in combination with Omron’s new NX I/O system and Sysmac NJ Controllers is a milestone and a decisive step towards the full integration of automation disciplines.
Learn more

Related events

Emballage

Discover our packaging innovations on EMBALLAGE, from 14th to 17th November 2016 in Paris Nord Villepinte exhibition halls. When: November 14 - 17, 2016
Where: Paris, France
Learn more

SPS/IPC/DRIVES

The SPS/IPC/DRIVES is Europe’s leading exhibition for electric automation. It covers all components down to complete systems and integrated automation solutions. More than 1,000 exhibitors will show their latest technologies in 14 halls from 22 to 24 November in the exhibition centre of Nürnberg. When: November 22 - 24, 2016
Where: Nürnberg, Germany
Learn more

SMART Industries

The second edition of the Smart Industries is expected to attract over 300 exhibitors to the Paris Nord Villepinte 8.000 square meter exhibition area. When: December 06 - 09, 2016
Where: Paris, France
Learn more