Industrial Automation
Industrial Automation | Europe
Country

Production ID system for the painting process

For the painting process several parameters are essential. How to deal with the harsh conditions in the paintshop.

The challenge

To identify the type of car in the painting process with a system that is resistant to the high temperature of the oven.

The solution

A RFID system is used to store the process parameters needed for the production of the car throughout the process. Harsh conditions through chemicals and high temperatures occur during the production steps. RFID is ideal for this application as it features high resistance tags for harsh conditions.

Added value

Main benefit of this system is that it is easy to set up and that it is resistant to temperatures up to 200°C.

Related products