Industrial Automation
Industrial Automation | Europe
Country

Displacement measurement of press machine mold

Correct alignment of press dies prevents defective molds.

The challenge

The challenge Occasionally misplacement of the mold resulted in defective molding. The required accuracy:
  • Tolerance: +/-50 micro meter
  • Resolution: +/-5 micro meter

The solution

Measure the displacement value of the mold and control the condition of forming. This is done with two laser displacement sensor heads and a multi-controller.
It is key in this application that the distance between the upper and lower dog (with two sensor heads) is measured this is possible due to the multi-controller.

Added value

Damage to the mold can be prevented, which makes production more efficient.

Related products