Industrial Automation
Industrial Automation | Europe
Country

Oven control

External influences can cause the temperature to deviate from the required set value. With the E5CN it is possible to programme the level at which display changes colour.
Alarm options include deviation from set point, where if the set point is changes the alarm moves with it. Absolute alarms where they are referenced to 0, standby so the alarms will not be active during the set point has been reached. Latching which means that once triggered they can only be deactivated by removing power.
This is ideal for remote or unmanned processes, as the alarm will remain until the machinery is next visited.

Related products