Industrial Automation
Industrial Automation | Europe
Country

Monitoring concentration

Monitoring the flow rate of the two liquids means that if one changes the other will match the change, with the offset required helping to maintain product quality.
The colour change display can be used to identify when the rate changes and additional alarm points can be set to give local or remote outputs. A linear output could be used for an input into a PLC system, SCADA or chart recorder if external monitoring or traceability are required.

Related products