Industrial Automation
Industrial Automation | Europe
Country

Wafer mapping

To detect wafers correctly use fiber heads with a narrow beam from which the tilt can be adjusted easily.

Challenge

To detect the presence of wafers in a wafer carrier correctly, the opening angle of through beam has to be narrow because of the unexpected reflection caused in the FOUP. Adjustment of the tilt of the narrow beam is difficult to achieve mechanically.

Solution

Omron offers fiber heads with a narrow beam (opening angle 1.5 degree) in which the tilt can be adjusted easily. The mounting reference-plane-based optical axis is already adjusted during the assembly, and the displacement is typically within 0.1 of a degree.

Benefit

Saves mapping-sensor adjustment time and offers stable mapping for high-yields.

Related products