Industrial Automation
Industrial Automation | Europe
Country

Bottle filling

It is very important to ensure that the correct number of tablets is placed into the bottle, so that the end patient receives the correct dosage. Fibre optics are used because of the possible variation is size.
The E3X fibre optic amplifiers can be used with a number of different sensing heads to give very small beams for detecting small objects. They can also be mounted in spaces inaccessible to traditional all in one sensors.
With a counting speed to upto 5kHz (5,000 counts per second) accuracy on high speed applications and with small parts such as tablets.
The output of the counter can be used to advance to the next container, and colour change will give a visual indication of when this should occur.

Related products